Read only
About VNA Options

MaximumSourceALCPower Property


Description

Returns a value indicating the maximum amount of source ALC power with 0 dB source attenuation.

To calculate the maximum amount of source ALC power with a different level of attenuation, subtract the amount source attenuation from this value.

 VB Syntax

value = cap.MaximumSourceALCPower (n)

Variable

(Type) - Description

value

(Double) - Variable to store the returned value for the maximum amount of source ALC power.

cap

A Capabilities (object)

n

(Long) - source number to query for maximum ALC power

Return Type

Double

Default

Not Applicable

Examples

value = cap.MaximumSourceALCPower'Read

C++ Syntax

HRESULT get_MaximumSourceALCPower(long sourceNum, double * power );

Interface

ICapabilities