Write/Read
About SA Application

MemShareEnabled Property


Description

Enables/disables exporting data to shared memory, which is the fastest way to transfer data between applications.

 VB Syntax

sa.dft.MemShareEnabled = value

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

value

(Boolean) Choose from:

0 - OFF - Disable memory sharing.

1 - ON - Enable memory sharing.

Return Type

Boolean

Default

OFF

Examples

sa.dft.MemShareEnabled = ON 'Write

value = sa.dft.MemShareEnabled 'Read

C++ Syntax

HRESULT get_MemShareEnabled(VARIANT_BOOL* enable)
HRESULT put_MemShareEnabled(VARIANT_BOOL enable)

Interface

ISpectrumAnalyzerDFT