Write/Read
About External DC Devices

MinOutput Property


Description

Sets and returns the "Define Min As" value for an external DC Source.

 VB Syntax

extDC.MinOutput = value

Variable

(Type) - Description

extDC

A ExternalDCDevice (object)

value

(Double) Minimum value for the external DC Source.

Return Type

Double

Default

-10 V

Examples

extDC.MinOutput = -10 'Write

value = extDC.MinOutput 'Read

C++ Syntax

HRESULT get_MinOutput( double* value);

HRESULT put_MinOutput( double value);

Interface

IExternalDCDevice3