Read only
About VNA Options

MinimumReceiverStepAttenuator Property


Description

Returns a value indicating the minimum amount of receiver attenuation.

 VB Syntax

value = cap.MinimumReceiverStepAttenuator (n)

Variable

(Type) - Description

value

(Double) - Variable to store the returned minimum value of receiver attenuation.

cap

A Capabilities (object)

n

(Long) - port number to query for minimum value of receiver attenuation

Return Type

Double

Default

Not Applicable

Examples

value = cap.MinimumReceiverStepAttenuator'Read

C++ Syntax

HRESULTget_ MinimumReceiverStepAttenuator(long portNumber,  double *  attenuation );

Interface

ICapabilities