| Write/Read | About iTMSA | 
| Description | Sets and returns the stimulus mode for balanced measurements. | 
| VB Syntax | balStim.Mode = value | 
| Variable | (Type) - Description | 
| balStim | A BalancedStimulus (object) | 
| value | (Enum NABALSTIMulus) - Stimulus Mode. True modes are applicable only with Opt S93460A/B - iTMSA. When a True-Mode is selected, the Balanced port powers are automatically uncoupled. Choose from: 0 - naSEStim: Single-Ended stimulus 1 - naTMStim: True-Mode stimulus 2 - naFTMStim: Forward only True-Mode stimulus 3 - naRTMStim: Reversed only True-Mode stimulus | 
| Return Type | Enum | 
| Default | 0 - naSEStim: Single-Ended stimulus | 
| Examples | balStim.Mode = naTMStim 'Write variable = balStim.Mode 'Read | 
| C++ Syntax | HRESULT get_Mode(tagNABALSTIMulus *eVal ); HRESULT put_Mode(tagNABALSTIMulus eVal ); | 
| Interface | IBalancedStimulus |