| Write/Read | About VNA-Pulse Generators | 
| Description | Sets the time lag between the pulse drive signal and the actual RF output. | 
| VB Syntax | pulse.ModulatorDelay = value | 
| Variable | (Type) - Description | 
| pulse | A PulseGenerator (object) | 
| value | (Double) - Modulator delay value. | 
| Return Type | Double | 
| Default | 40 ns | 
| Examples | pulse.ModulatorDelay = 40ns 'Write | 
| value = pulse.ModulatorDelay 'Read | |
| C++ Syntax | HRESULT get_ModulatorDelay(double* val); HRESULT put_ModulatorDelay(double val); | 
| Interface | IPulseGenerator5 |