Write/Read |
About External Devices |
Description |
Sets and returns the name of the External Device. |
VB Syntax |
extDev.Name = value |
Variable |
(Type) - Description |
extDev |
A ExternalDevice Object (object). |
value |
(string) - External Device name. Any string name limited to alpha-numeric characters. |
Return Type |
String |
Default |
Device<n> |
Examples |
extDev.Name = "MySource" 'Write |
extDevName = extDev.Name 'Read See example program to configure PMAR device See example program to configure External Source |
|
C++ Syntax |
HRESULT get_Name(BSTR *pVal) HRESULT put_Name(BSTR newVal) |
Interface |
IExternalDevice |