Write/Read
About Traces

Name (trace) Property


Description

Sets or returns the name of the Trace. Use the trace name to identify the trace and refer to the trace in the collection.

Note: This is the same name as meas.Name; when one changes, the other changes.

 VB Syntax

trac.Name = value

Variable

(Type) - Description

trac

A Trace (object)

value

(String) Trace name

Return Type

String

Default

"CH1_S11_1" - name of the default measurement

Examples

trace.Name = "myTrace" 'Write

traceName = Name.Trace 'Read

C++ Syntax

HRESULT put_Name(BSTR name)
HRESULT get_Name(BSTR *name)

Interface

ITrace