Write/Read |
About Noise Figure |
Description |
Sets and reads the averaging of the noise receiver. |
VB Syntax |
noise.NoiseAverageFactor = value |
Variable |
(Type) - Description |
noise |
A NoiseFigure (object) |
value |
(long integer) - Averaging value. Choose a number between 1 and 99. |
Return Type |
Long Integer |
Default |
1 |
Examples |
noise.NoiseAverageFactor = 10 'Write |
AvgNoise = noise.NoiseAverageFactor 'Read |
|
C++ Syntax |
HRESULT get_NoiseAverageFactor(long* pVal) HRESULT put_NoiseAverageFactor(long newVal) |
Interface |
INoiseFigure |