Read only
About VNA Options

NoiseReceiverNoiseBWList  Property


Description

Returns the list of supported Noise Bandwidths values when using a noise receiver (option 029). Learn more about Opt. 029.

 VB Syntax

value = cap.NoiseReceiverNoiseBWList

Variable

(Type) - Description

value

Variant containing one-dimensional array of long integers.

cap

A Capabilities (object)

Default

Not Applicable

Examples

value = cap.NoiseReceiverNoiseBWList  'Read

C++ Syntax

HRESULT get_NoiseReceiverNoiseBWList (Variant *list);

Interface

ICapabilities13