Write/Read
About Noise Figure

NoiseReceiver Property


Description

Sets and returns the receiver to use for noise measurements.

 VB Syntax

noise.NoiseReceiver = value

Variable

(Type) - Description

noise

A NoiseFigure (object)

value

(Enum as NANoiseReceiverMode) Noise receiver. Choose from:

0 - naStandardReceiver The standard VNA receiver. (Opt 028 or 029)

1 - naNoiseReceiver  The noise receiver. (Opt 029 ONLY)

Return Type

Enum

Default

1 - naNoiseReceiver

Examples

noise.NoiseReceiver = naNoiseReceiver 'Write

NoiseRec = noise.NoiseReceiver 'Read

C++ Syntax

HRESULT get_NoiseReceiver(tagNoiseReceiverMode *pVal);

HRESULT put_NoiseReceiver(tagNoiseReceiverMode newVal);

Interface

INoiseFigure5