Write/Read
About Noise Figure

NoiseSourceCold Property


Description

Sets and returns the temperature of the noise source connector.

 VB Syntax

noise.NoiseSourceCold = value

Variable

(Type) - Description

noise

A NoiseCal (object)

value

(double) Noise source temperature in Kelvin.

Return Type

Double

Default

Not Applicable

Examples

noise.NoiseSourceCold = 295 'Write

temp = noise.NoiseSourceCold 'Read

C++ Syntax

HRESULT get_NoiseSourceCold(double* pTemp)

HRESULT put_NoiseSourceCold(double pNewTemp)

Interface

INoiseCal