Write/Read
About Noise Figure

NoiseTunerIn Property


Description

Sets and returns the port identifier of the ECal noise tuner that is connected to the VNA Source.

 VB Syntax

noise.NoiseTunerIn = value

Variable

(Type) - Description

noise

A NoiseFigure (object)

value

(string) Noise Tuner port identifier that is connected to the VNA source, as it is labeled on the ECal module. For example, for 2-port ECal modules, choose either "A" or "B".

Return Type

String

Default

Not Applicable

Examples

noise.NoiseTunerIn = "A"'Write

EcalPort = noise.NoiseTunerIn 'Read

C++ Syntax

HRESULT get_NoiseTunerIn(BSTR* pValue)

HRESULT put_NoiseTunerIn(BSTR pNewValue)

Interface

INoiseFigure