Write/Read
About Noise Figure

NoiseTunerOut Property


Description

Sets and returns the port identifier of the ECal noise tuner that is connected to the DUT.

 VB Syntax

noise.NoiseTunerOut = value

Variable

(Type) - Description

noise

A NoiseFigure (object)

value

(string) Noise Tuner port identifier that is connected to the DUT, as it is labeled on the ECal module. For example, for 2-port ECal modules, choose either "A" or "B".

Return Type

String

Default

Not Applicable

Examples

noise.NoiseTunerOut = "A"'Write

EcalPort = noise.NoiseTunerOut 'Read

C++ Syntax

HRESULT get_NoiseTunerOut(BSTR* pValue)

HRESULT put_NoiseTunerOut(BSTR pNewValue)

Interface

INoiseFigure