Write/Read |
About Gain Compression |
Description |
Set and read the number of frequency points for a Gain Compression channel. Applies to all acquisition modes. |
VB Syntax |
gca.NumberOfFrequencyPoints = value |
Variable |
(Type) - Description |
gca |
A GainCompression (object) |
value |
(integer) - Frequency points. Do not exceed the max number of points. Learn more. |
Return Type |
Integer |
Default |
201 |
Examples |
gca.NumberOfFrequencyPoints = 101 'Write |
freqPts = gca.NumberOfFrequencyPoints 'Read |
|
C++ Syntax |
HRESULT get_NumberOfFrequencyPoints(int* pVal) HRESULT put_NumberOfFrequencyPoints(int newVal) |
Interface |
IGainCompression |