Read-only
About Embedded LO

NumberOfSweeps Property


Description

Returns the number of tuning sweeps used for the latest embedded LO measurement.

 VB Syntax

value = embedLODiag.NumberOfSweeps

Variable

(Type) - Description

value

(Long) Variable to store the returned data.

embedLODiag

An EmbeddedLODiagnostic (object)

Return Type

(Long)

Default

Not Applicable

Examples

data= embedLODiag.NumberOfSweeps 'read

C++ Syntax

HRESULT get_NumberOfSweeps(long * numSweeps);

Interface

IEmbededLODiagnostic