| Read-only | 
 | 
| Description | Returns the number of data points of the measurement. To understand how this property is useful, see IMeasurement2 Interface. | 
| VB Syntax | value = meas.NumberOfPoints | 
| Variable | (Type) - Description | 
| value | (Long) - variable to store the returned value | 
| meas | A Measurement (object) | 
| Return Type | Long Integer | 
| Default | Not Applicable | 
| Examples | Print meas.NumberOfPoints 'prints the number of data points | 
| C++ Syntax | HRESULT get_NumberOfPoints(long *pVal); | 
| Interface | IMeasurement2 |