Read-only
About Spectrum Analyzer Markers

OccupiedBandCenter Property


Description

Returns the occupied bandwidth center frequency.

 VB Syntax

value = mkr.OccupiedBandCenter

Variable

(Type) - Description

value

Variable to store the center frequency value.

mkr

A Marker (object)

Return Type

Double

Default

Not Applicable

Examples

value = mkr.OccupiedBandCenter 'Read

C++ Syntax

HRESULT get_OccupiedBandCenter(double* pVal)

Interface

IMarker7