Write/Read |
About Spectrum Analyzer Markers |
Description |
Returns the occupied bandwidth span. |
VB Syntax |
value = mkr.OccupiedBandSpan |
Variable |
(Type) - Description |
value |
Variable to store the span value. |
mkr |
A Marker (object) |
Return Type |
Double |
Default |
Not Applicable |
Examples |
value = mkr.OccupiedBandSpan 'Read |
C++ Syntax |
HRESULT get_OccupiedBandSpan(double* pVal) |
Interface |
IMarker7 |