Write/Read
About Spectrum Analyzer Markers

OccupiedBandState Property


Description

Sets and returns the occupied bandwidth on/off state.

 VB Syntax

mkr.OccupiedBandState  = value

Variable

(Type) - Description

mkr

A Marker (object)

value

(Enum as NaStates) - Choose from:

naOFF (0) - Turns occupied bandwidth OFF.

naON (1) - Turns occupied bandwidth ON.

Return Type

Enum

Default

naOFF (0)

Examples

mkr.OccupiedBandState = naON 'Write

obwstate = mkr.OccupiedBandState 'Read

C++ Syntax

HRESULT OccupiedBandState(tag NAStates* pState);
HRESULT OccupiedBandState(tag NAStates pState)

Interface

IMarker7

Note: If occupied band state is turned ON, then Band Power or Band Noise is turned OFF.