Write/Read |
About Marker Readout |
Description |
Either show marker readout of only the active trace or all of the traces simultaneously. Note: This method is replaced by MarkerReadoutsPerTrace Property |
VB Syntax |
win.OneReadoutPerTrace = state |
Variable |
(Type) - Description |
win |
A NAWindow (object) |
value |
(boolean) True - Shows the readout of only the active marker for each trace. False - Shows up to 5 marker readouts per trace, up to 20 total readouts. |
Return Type |
Boolean |
Default |
False |
Examples |
win.OneMarkerReadoutPerTrace = True 'Write State = app.ActiveNAWindow.OneMarkerReadoutPerTrace 'Read |
C++ Syntax |
HRESULT get_OneMarkerReadoutPerTrace(VARIANT_BOOL *pVal) HRESULT put_OneMarkerReadoutPerTrace(VARIANT_BOOL newVal) |
Interface |
INAWindow |