Write/Read
About Testset Control

OutputPort Property


Description

Switches an input to one of the valid outputs on the specified E5091A. The following are valid input/output combinations. If a combination other than these are sent, an “invalid argument” error will occur.

Input

Valid Outputs

1

A

T1- If Port 2 already is connected to T1, then Port 2 will be switched to T2.)

2

T1 - If Port 1 already is connected to T1, then Port 1 will be switched to A.

T2

3

R1+

R2+

R3+   If option 007 (7port), R2 is selected.

4

R1-

R2-

R3-   If option 007 (7port), R2 is selected.

Note: Do not confuse the similar Testset.OutputPorts Property, which sets or gets the port mapping for ALL ports.

 VB Syntax

testsets(1).OutputPort (chNum,input) = output

Variable

(Type) - Description

testsets(1)

An item from Testsets (collection)

Learn how to identify a testset in the collection.

chNum

(Long)  Channel number of the measurement.

input

(Long) Testset Input port. Choose from 1|2|3|4.

output

(Enum as NAE5091OutputPort) Output port to switch to specified Input. Choose from:

0 or naE5091PortA -  Port A

1 or naE5091PortT1 - Port T1

2 or naE5091PortT2 - Port T2

3 or naE5091PortR1 - Port R1

4 or naE5091PortR2 - Port R2

5 or naE5091PortR3 - Port R3

Return Type

Enum

Default

Not Applicable

Examples

See Example Program

C++ Syntax

HRESULT get_OutputPort(long channelNum, long inputPort, E5091OutputPort *outPort);
HRESULT put_OutputPort(long channelNum, long inputPort, E5091OutputPort outPort);

Interface

IE5091Testsets