Read-only |
About Diff I/Q App |
Description |
Returns a list of all existing parameters. |
VB Syntax |
params = DIQ.ParameterList |
Variable |
(Type) - Description |
params |
(Variant Array) Comma-separated list of parameters, each parameter in the form “name:expression”. |
DIQ |
A Differential I/Q (object) |
Return Type |
(Variant Array) |
Default |
Not Applicable |
Example |
params = diq.ParameterList 'Read 'Returns "IPwrF1:a1_F1","OPwrF1:b2_F1","GainF1:b2_F1/a1_F1" |
C++ Syntax |
HRESULT get_ParameterList(VARIANT* params); |
Interface |
IDIQ |