Read-only
 

Parameter Property


Description

Returns the measurement Parameter. To change the parameter, use meas.ChangeParameter

 VB Syntax

measPar = meas.Parameter

Variable

(Type) - Description

measPar

(string) - Variable to store Parameter string

meas

A Measurement (object)

Return Type

String

Default

Not applicable

Examples

measPar = meas.Parameter 'Read

C++ Syntax

HRESULT get_Parameter(BSTR *pVal)

Interface

IMeasurement