Write/Read
About Marker Search

PeakExcursion Property


Description

Sets and reads the peak excursion value for the specified marker. The Excursion value determines what is considered a "peak".

 VB Syntax

mark.PeakExcursion = value

Variable

(Type) - Description

mark

A Marker (object)

value

(single) - Peak Excursion. Choose any number between -500 and 500

Return Type

Single

Default

3

Examples

mark.PeakExcursion = 1 'Write

PkExcur = mark.PeakExcursion 'Read

C++ Syntax

HRESULT get_PeakExcursion(float *pVal)
HRESULT put_PeakExcursion(float newVal)

Interface

IMarker