Write/Read
About Group Delay

Percent Property


Description

Sets group delay aperture using a percent of the channel frequency span.

 VB Syntax

gdAperture.Percent = value

Variable

(Type) - Description

gdAperture

A GroupDelayAperture (object)

value

(Double) Percent of frequency span to use for the aperture setting. Choose between the equivalent of 2 points and 100 percent of the channel frequency span.

Return Type

Double

Default

Percent range that equates to 11 points.

This can be changed to two points with a preference setting.

Examples

gdAperture.Percent = 25 'Write

aperture = gdAperture.Percent 'Read

C++ Syntax

HRESULT get_Percent(double Percent *pVal)

HRESULT put_Percent(double Percent newVal)

Interface

IGroupDelayAperture