Write/Read
About Diff I/Q App

PhaseSweepState Property


Description

Sets and reads the ON / OFF state of phase sweep.

On the Source Configuration dialog under Phase, this is the Sweep Phase (On|Off) setting.

 VB Syntax

DIQ.PhaseSweepState (port) = value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

port

(String) Source port name. Use SourcePortNames to read a list of valid source ports.

value

(Boolean)  Choose from:

  • True - Sweep phase.

  • False - Do not sweep phase.

Return Type

Boolean

Default

False

Examples

oDIQ.PhaseSweepState("port 2") = True

Value = oDIQ.PhaseSweepState("port 2") 'Read

C++ Syntax

HRESULT get_PhaseSweepState(BSTR port, BOOL* PhaseSweepState);

HRESULT put_PhaseSweepState(BSTR port, BOOL PhaseSweepState);

Interface

IDIQ