Write/Read
About Phase Sweep

PhaseSwpState Property


Description

Sets and reads the state of phase sweep. Sweep type must be set to CWTime.

 VB Syntax

balStim.PhaseSwpState  = value

Variable

(Type) - Description

balStim

A BalancedStimulus (object)

value

(Boolean) State of phase sweep.

False   Phase sweep disabled.

True  Phase sweep enabled.

Return Type

Boolean

Default

False

Examples

balStim.PhaseSwpState = False 'Write

var = balStim.PhaseSwpState   'Read

C++ Syntax

HRESULT get_PhaseSwpState (VARIANT_BOOL *bVal)

HRESULT put_PhaseSwpState (VARIANT_BOOL bVal)

Interface

IBalancedStimulus2