Write/Read |
About Group Delay |
Description |
Sets group delay aperture using a fixed number of data points. |
VB Syntax |
gdAperture.Points = value |
Variable |
(Type) - Description |
gdAperture |
A GroupDelayAperture (object) |
value |
(Double) Number of data points to use for the aperture setting. Choose between two points and the number of points in the channel. |
Return Type |
Double |
Default |
Points range that equates to 11 points. This can be changed to two points with a preference setting. |
Examples |
gdAperture.Points = 25 'Write |
aperture = gdAperture.Points 'Read |
|
C++ Syntax |
HRESULT get_Points(double Points *pVal) HRESULT put_Points(double Points newVal) |
Interface |
IGroupDelayAperture |