Write/Read |
About Segment Sweep |
Description |
Sets or returns the IF Bandwidth per port property of the Segment. Enable the IF bandwidth per port property using the PortIFBandwidthOption Property of the Segments collection. |
VB Syntax |
seg.PortIFBandwidth(port) = value |
Variable |
(Type) - Description |
seg |
A Segment (object) |
port |
(Long) Port number. |
value |
(Double) IF bandwidth. |
Return Type |
Double |
Default |
1000 |
Examples |
seg.PortIFBandwidth(1) = 1000 'Write |
value = seg.PortIFBandwidth(1) 'Read |
|
C++ Syntax |
HRESULT get_PortIFBandwidth(long port, double* pVal); HRESULT put_PortIFBandwidth(long port, double pVal); |
Interface |
ISegment3 |