Write/Read
About Modifying Cal Kits

PortLabel Property


Description

Sets and returns the label on the calibration kit Port for the calibration wizard.

 VB Syntax

calKit.Portlabel (portNum) = value

Variable

(Type) - Description

calKit

A CalKit (object)

portNum

(long integer) - number of the port to be labeled. Choose either 1 or 2

value

(string) - Label that is visible in the calibration wizard.

Return Type

String

Default

Depends on the Cal Kit.

Examples

calKit.PortLabel = "MyCalKit" 'Write

kitLabel = calKit.PortLabel 'Read

C++ Syntax

HRESULT get_PortLabel(long port, BSTR *pVal)
HRESULT put_PortLabel(long port, BSTR newVal)

Interface

ICalKit