Read/Write
About Dynamic Uncertainty

PortNoiseEnabled Property


Description

Sets and returns the ON/OFF state of allowing noise data to contribute to the uncertainty of a calibration performed using Dynamic Uncertainty. Noise data must also be present for the ports at the time the calibration is performed.

VB Syntax

uncertMan.PortNoiseEnabled = value

Variable

(Type) - Description

uncertMan

An UncertaintyManager Object

value

(Boolean) Noise contribution state. Choose from:

True - Noise uncertainty ON.

False - Noise uncertainty OFF.

Return Type

Boolean

Default

True

Examples

uncertMan.PortNoiseEnabled = True

See example program

C++ Syntax

HRESULT get_PortNoiseEnabled([out,retval] VARIANT_BOOL* pState);

HRESULT put_PortNoiseEnabled([in] VARIANT_BOOL state);

Interface

IUncertaintyManager