Write/Read
About Diff I/Q App

PortPhaseStop Property


Description

Sets and reads the Stop value for a phase sweep.

On the Source Configuration dialog under Phase, this is the Stop Phase setting.

 VB Syntax

DIQ.PortPhaseStop (port) = value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

port

(String) Source port name. Use SourcePortNames to read a list of valid source ports.

value

(Double)  Stop phase sweep value in degrees. Choose any positive or negative value.

Return Type

Double

Default

0

Examples

oDIQ.PortPhaseStop("port 2") = -90

Value = oDIQ.PortPhaseStop("port 2") 'Read

C++ Syntax

HRESULT get_PortPhaseStop(BSTR port, double* PortPhaseStop);

HRESULT put_PortPhaseStop(BSTR port, double PortPhaseStop);

Interface

IDIQ