Write/Read
About Diff I/Q App

PortStartPower Property


Description

Sets and reads the start value of a power sweep.

On the Source Configuration dialog under Power, this is the Start Power setting.

 VB Syntax

DIQ.PortStartPower (port) = value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

port

(String) Source port name. Use SourcePortNames to read a list of valid source ports.

value

(Double)  Power sweep start value in dBm. Choose start and stop value within a single attenuator range of the analyzer (generally about 30 dB).

Return Type

Double

Default

-5 dBm

Examples

oDIQ.PortStartPower("port 2") = 0

Value = oDIQ.PortStartPower("port 2") 'Read

C++ Syntax

HRESULT get_PortStartPower(BSTR port, double* PortStartPower);

HRESULT put_PortStartPower(BSTR port, double PortStartPower);

Interface

IDIQ