Write/Read
About Diff I/Q App

PortStopPower Property


Description

Sets and reads the stop value of a power sweep.

On the Source Configuration dialog under Power, this is the Stop Power setting.

 VB Syntax

DIQ.PortStopPower (port) = value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

port

(String) Source port name. Use SourcePortNames to read a list of valid source ports.

value

(Double)  Power sweep stop value in dBm. Choose start and stop value within a single attenuator range of the analyzer (generally about 30 dB).

Return Type

Double

Default

-5 dBm

Examples

oDIQ.PortStopPower("port 2") = 0

Value = oDIQ.PortStopPower("port 2") 'Read

C++ Syntax

HRESULT get_PortStopPower(BSTR port, double* PortStopPower);

HRESULT put_PortStopPower(BSTR port, double PortStopPower);

Interface

IDIQ