Read-only |
About Source Power CalAbout PMAR |
Description |
Returns the power uncertainty associated with the specific power meter at the specified frequency and power. |
VB Syntax |
pwrUnc = pwrSensor.PowerMtrReadingUncertainty(freq,power) |
Variable |
(Type) - Description |
pwrUnc |
(Double) Variable to store the returned power meter reading uncertainty. |
pwrSensor |
A PowerSensorUncertainty (Object) |
freq |
(Double) Frequency (Hz). |
power |
(Double) Power (dBm). |
Return Type |
Double (Watts) |
Default |
Not Applicable |
Examples |
pwrUnc = pwrSensor.PowerMtrReadingUncertainty(10e9,0.0) |
C++ Syntax |
HRESULT PowerMtrReadingUncertainty(double freq, double power, double *pwrUnc); |
Interface |
IPowerSensorUncertainty |