Write/Read
About RF power during sweep retrace

PowerOnDuringRetraceMode Property


Description

For single-band frequency or segment sweeps ONLY, specify whether to turn RF power ON or OFF during a retrace.

This setting remains until changed using this command, or until the hard drive is changed or reformatted.

 VB Syntax

pref.PowerOnDuringRetraceMode = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(Enum) - Choose from:

0 - naRetracePowerMode_Auto Power is left ON during retrace of single-band frequency or segment sweeps ONLY.

1 - naRetracePowerMode_OFF  Power is turned OFF during retrace of single-band frequency or segment sweeps ONLY.

Return Type

Enum

Default

0 - naRetracePowerMode_Auto

Examples

pref.PowerOnDuringRetraceMode = naPowerSweepRetraceMode_Start 'Write

psMode = pref.naPowerOnDuringRetraceMode_Start 'Read

C++ Syntax

HRESULT get_PowerOnDuringRetraceMode (tagNARetracePowerMode* preference);
HRESULT put_PowerOnDuringRetraceMode (tagNARetracePowerMode val)

Interface

IPreferences4