Write / Read |
About Receiver Leveling |
Description |
Sets and reads the type of power range data (specified or typical) to be returned. |
VB Syntax |
powerRange.PowerRangeType = value |
Variable |
(Type) - Description |
powerRange |
A PowerRange (object) |
value |
(Enum NAType) Choose from: 0 or naSpecifiedPower 1 or naTypicalPower |
Return Type |
Enum |
Default |
Not Applicable |
Examples |
powerRange.PowerRangeType = naSpecifiedPower 'Write |
C++ Syntax |
HRESULT get_PowerRangeType(enum NAType *val); HRESULT put_PowerRangeType(enum NAType val); |
Interface |
IPowreRange |