Read/Write |
About Embedded LO |
Description |
Sets and returns the tuning tolerance for precise tuning. |
VB Syntax |
obj.PreciseTuningTolerance = value |
Variable |
(Type) - Description |
obj |
An EmbeddedLO (object) or A ConverterEmbeddedLO (object) |
value |
(Double) Tuning tolerance in Hz. |
Return Type |
(Double) |
Default |
1 Hz |
Examples |
embedLO.PreciseTuningTolerance = .5 'write |
value = embedLO.PreciseTuningTolerance 'read |
|
C++ Syntax |
HRESULT get_PreciseTuningTolerance(double* tolerance); HRESULT put_PreciseTuningTolerance(double tolerance); |
Interface |
IEmbededLO |