Write/Read |
About Receiver Overload |
Description |
Set and return whether to turn source power OFF when a receiver is overloaded. |
VB Syntax |
pref.RFOffOnReceiverOverload = value |
Variable |
(Type) - Description |
pref |
A Preferences (object) |
value |
(Boolean) - Choose from: True Turn OFF source power to ALL ports when a receiver is overloaded. False Power remains ON when a receiver is overloaded. |
Return Type |
Boolean |
Default |
False |
Examples |
pref.RFOffOnReceiverOverload = True 'Write |
value = pref.RFOffOnReceiverOverload 'Read |
|
C++ Syntax |
HRESULT get_RFOffOnReceiverOverload (VARIANT_BOOL* preference); |
Interface |
IPreferences12 |