Read-only
About FOM

RangeCount Property


Description

Returns the number of ranges that are available in the VNA.

To see the range names, query the Name property of each range in the FOM  collection.

 VB Syntax

value = FOM.RangeCount

Variable

(Type) - Description

object

An FOM (collection object)

value

(long) - Variable to store the returned number of ranges.

Return Type

Long Integer

Default

Not Applicable

Examples

NumRanges = fom.RangeCount 'Read

C++ Syntax

HRESULT get_RangeCount(long *count)

Interface

IFOM