Write/Read
About Diff I/Q App

RangeDivisor Property


Description

Sets and reads the value by which the coupled range will be divided to achieve the frequency range specified by <rNum>.

On the Frequency Range dialog under Coupling, this is the Divisor setting.

 VB Syntax

DIQ.RangeDivisor (n) = value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

n

(Long Integer) Frequency range number.

value

(Long Integer) Divisor value. Choose a positive or negative integer.

Return Type

Long

Default

1

Examples

diq.RangeDivisor 2 = 2 'Write

value = diq.RangeDivisor 2 'Read

C++ Syntax

HRESULT get_RangeDivisor(long range, long* RangeDivisor);

HRESULT put_RangeDivisor(long range, long RangeDivisor);

Interface

IDIQ