Write/Read
About Diff I/Q App

RangeIFBW Property


Description

Sets and reads the receiver IF bandwidth setting.

On the Frequency Range dialog under Frequency, this is the IFBW setting.

 VB Syntax

DIQ.RangeIFBW (n) = value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

n

(Long Integer) Frequency range number.

value

(Double) IF Bandwidth in Hz. The list of valid IF Bandwidths is different depending on the analyzer model. (See the list.) If an invalid number is specified, the analyzer will round up to the closest valid number.

Return Type

Double

Default

1e5

Examples

diq.RangeIFBW 1 = 1e3 'Write

value = diq.RangeIFBW 'Read

C++ Syntax

HRESULT get_RangeIFBW(long range, double* RangeIFBW);

HRESULT put_RangeIFBW(long range, double RangeIFBW);

Interface

IDIQ