Write/Read
About Receiver Leveling

RangeStartFrequency (PowerRange) Property


Description

Sets and reads the lower bound of the frequency range used for range based power min and max.

 VB Syntax

powerRange.RangeStartFrequency = value

Variable

(Type) - Description

powerRange

A PowerRange (object)

value

(Double) Start frequency. Choose a number within the frequency limits of the analyzer. Units are Hz.

Return Type

Double

Default

Not Applicable

 

powerRange.RangeStartFrequency = 1e9 'Write
value = powerRange.RangeStartFrequency 'Read

C++ Syntax

HRESULT get_RangeStartFrequency(double* startfreq);

HRESULT put_RangeStartFrequency(double startfreq);

Interface

IPowreRange