Write/Read
About Receiver Leveling

RangeStopFrequency (PowerRange) Property


Description

Sets and reads the upper bound of the frequency range used for range based power min and max.

 VB Syntax

powerRange.RangeStopFrequency = value

Variable

(Type) - Description

powerRange

A PowerRange (object)

value

(Double) Stop frequency. Choose a number within the frequency limits of the analyzer. Units are Hz.

Return Type

Double

Default

Not Applicable

 

powerRange.RangeStopFrequency = 10e9 'Write
value = powerRange.RangeStopFrequency 'Read

C++ Syntax

HRESULT get_RangeStopFrequency(double* stopfreq);

HRESULT put_RangeStopFrequency(double stopfreq);

Interface

IPowreRange