Write / Read |
About Source Power CalAbout PMAR |
Description |
This command, along with ReadingsPerPoint Property allows for settling of the power sensor READINGS. Each power reading is averaged with the previous readings at each stimulus point. When the average meets this tolerance value or the maximum ReadingsPerPoint has been made, the average is returned as the valid reading. |
VB Syntax |
pwrSens.ReadingsTolerance = value |
Variable |
(Type) - Description |
|
pwrCal |
A SourcePowerCalibrator (Object) or A PowerSensorAsReceiver (Object) |
|
value |
(Double) – Power meter settling tolerance value in dB. Choose any number between 0 and 5. |
Return Type |
Double |
Default |
.05 dB |
Examples |
pwrSens.ReadingsTolerance = .1 'Write |
C++ Syntax |
HRESULT get_ReadingsTolerance( double *pVal); HRESULT put_ReadingsTolerance( double newVal); |
Interface |
ISourcePowerCalibrator3 IPowerSensorAsReceiver |