Read-only | 
About External Trigger | 
Description | 
 Checks if the PNA is ready for a hardware trigger. This command is not intended to be used in a dynamic triggering situation where the ready status is constantly changing. Instead, the expected use is a more static situation where you are expecting the PNA to transition from not ready to ready, and then wait for a trigger. The PNA is polled until it becomes ready and then an operation that triggers the PNA is performed. Note: This command is only supported on the PNA-L, PNA, and PNA-X with DSP5 installed. Any other model will return an error.  | 
VB Syntax | 
 value = trigsetup.ReadyForTriggerStatus  | 
Variable | 
(Type) - Description | 
| 
 trigsetup  | 
 A TriggerSetup (object)  | 
| 
 value  | 
 (Enum as NATriggerReadyStatusSource) 0 - naTriggerAny - Check if the PNA is ready for any of the following hardware triggers. 1 - naTriggerMeas - Check if the PNA is ready for an External trigger from the Meas Trig In BNC, Handler IO Pin 18, or Pulse 3 line. 2 - naTrigger Aux1 - Check if the PNA is ready for a trigger from the AUX TRIG 1 IN on the rear panel. 3 - naTriggerAux2 - Check if the PNA is ready for a trigger from the AUX TRIG 2 IN on the rear panel.  | 
Return Type | 
 Boolean  | 
Default | 
 Not applicable  | 
| 
 
  | 
 value = trigsetup.ReadyForTriggerStatus 0 'Read  | 
C++ Syntax | 
 HRESULT get_ReadyForTriggerStatus(tagNATriggerReadyStatusSource whichTrigger, VARIANT_BOOL* val);  | 
Interface | 
 ITriggerSetup4  |