Description |
Returns the receiver (response) port number of measurement. To understand how this property is useful, see IMeasurement2 Interface. Note: Returning a receiver port is only supported for S-Parameter measurements. If the measurement is not an S-Parameter, then E_NA_BAD_PARAMETER is returned. |
VB Syntax |
value = meas.ReceivePort |
Variable |
(Type) - Description |
value |
(Long) - Variable to store the returned value |
meas |
A Measurement (object) |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
rp = meas.ReceivePort |
C++ Syntax |
HRESULT ReceivePort(Long* rcvPort); |
Interface |
IMeasurement2 |