Read only
About Receiver Temp

ReceiverTemperature Property


Description

Returns the current temperature on the VNA receiver board.

 VB Syntax

value = cap.ReceiverTemperature (unit)

Variable

(Type) - Description

value

(Double) - Variable to store the returned temperature value.

cap

A Capabilities (object)

unit

(Enum as NATempScale) - Units in which temperature is returned. Choose from:

  • 0 - naTempScale_Fahrenheit

  • 1 - naTempScale_Celsius

Return Type

Double

Default

Not Applicable

Examples

value = cap.ReceiverTemperature naTempScale_Celsius'Read

C++ Syntax

HRESULT get_ReceiverTemperature(NATempScale val, long temperature);

Interface

ICapabilities9