Write/Read
About Receiver Attenuation

ReceiverAttenuator Property


Description

Sets or returns the value of the specified receiver attenuator control.

 VB Syntax

object.ReceiverAttenuator(rec) = value

Variable

(Type) - Description

object

Channel (object)

or

CalSet (object) - Read-only property

rec

(long integer) - Receiver with attenuator control to be changed. Choose from any of the available receivers in your VNA

1 - Receiver A

2 - Receiver B

3 - Receiver C

4 - Receiver D

Receiver attenuation can not be set using logical receiver notation.

value

(double) - Attenuator value in dB. Choose any Long Integer between 0 and 35 in 5dB steps:

If an invalid value is entered, the analyzer will select the next lower valid value. For example, if 19.9 is entered the analyzer will select 15 dB attenuation.

Return Type

Double

Default

0 db

Examples

chan.ReceiverAttenuator(1) = 5 'Write

attn = chan.ReceiverAttenuator(2) 'Read

C++ Syntax

HRESULT get_ReceiverAttenuator(long lport, double* pVal)
HRESULT put_ReceiverAttenuator(long lport, double newVal)

Interface

IChannel

|CalSet3